Technical FAQs

Ask a Question

Is there a restriction as to where a 125 amp 3 pole ED, EG, or EJ breaker can be mounted in a 250 amp max NF interior?

Yes, it can only be installed at the bottom on either side .

CTA-ID : 10720
Was this helpful?
What can we do to improve the information ?