Technical FAQs

Ask a Question

Can I mount (2) three pole ED, EG, or EJ 125 amp breakers in a 250 amp maximum panel?

No, only one 125 amp three pole ED, EG, or EJ breaker can be installed on a 250 amp NF panel.


CTA-ID : 10719
Was this helpful?
What can we do to improve the information ?