Technical FAQs

Ask a Question

In the MPS 10`` wide NQOB and NF column width panel, with the increased panel width can I get a larger than 60 amp branch breaker ?

No. The panel was not retested so the testing results remain the same as for the standard 8 5/8`` column width enclosure. The additional space on each side of the interior is only half of the total increased space so there would be no appreciable increase in wire bending space. A 60A breaker is the maximum branch breaker.


CTA-ID : 10694
Was this helpful?
What can we do to improve the information ?