Technical FAQs

Ask a Question

Is 24 volt replacement control coil available for LC1D11500?

Yes, order LX1D8B5 for 50 hertz, LX1D8B6 for 60 hertz or LX1D8B7 for 50/60 hertz. Average coil consumption is 300 VA inrush 22 VA sealed for 50 hertz, 300 VA inrush 22 VA sealed for 60 hertz and 280 to 350 VA inrush 2 to 18 VA sealed for 50/60 hertz.


CTA-ID : 11157
Was this helpful?
What can we do to improve the information ?