Technical FAQs

Ask a Question

On a SDM11VMH Channel Injector, what position of the screw-down terminal strip is used for each pair of the Category 5 wire?

If using Category-5, 4 UTP (Unshielded Twisted Pair):
Position 1 = Brown
Position 2 = Brown/White
Position 3 = Green
Position 4 = Green/White
Position 5 = Orange
Position 6 = Orange/White
Position 7 = Blue
Position 8 = Blue/White
If using Quad (4 conductor) ``station wire``:
Position 3 = Yellow
Position 4 = Black
Position 7 = Red
Position 8 = Green
Positions 1,2, 5 and 6 will not be used if terminating Quad wire.


CTA-ID : 10880
Was this helpful?
What can we do to improve the information ?