Technical FAQs

Ask a Question

On a SDM11VMB Channel Injector, what function is provided by each pair of the Category-5 wire?

If using Category-5, 4 UTP (Unshielded Twisted Pair) wire, the Brown/Brown-White pair is the Audio Pair. The Green/Green-White pair is the Video pair. The Orange/Orange-White pair is the Sense Pair (senses length of Cat-5 wire run). The Blue/Blue-White pair is the 12V Power Pair.
If using Quad wire, the Yellow and Black wires are the Video pair. The Red and Green wires are the 12V Power Pair.


CTA-ID : 10877
Was this helpful?
What can we do to improve the information ?