Technical FAQs

Ask a Question

What Class of fuse does the H268, H268R and H268AWK safety switches accept?

These switches accept Class L fuses only. With Class L fuses installed, the switches are UL listed for use on systems with up to 200,000 RMS Symmetrical Amperes available fault current.


CTA-ID : 11107
Was this helpful?
What can we do to improve the information ?