Technical FAQs

Ask a Question

What are the ground-fault detection features of the AFI breaker?

The AFI breakers will detect ground-faults with 30-50 mA of leakage to ground, but they are not listed, labeled, or advertised as ground fault protectors. If GFI protection is required, the present AFI breaker is not acceptable.

CTA-ID : 10405
Was this helpful?
What can we do to improve the information ?