Technical FAQs

Ask a Question

Is 208 volt replacement control coil available for LC1D2510?

Yes, order LX1D4L6 for 60 hertz. Average coil consumption is 90 VA inrush 7.5 VA sealed for 50 hertz, 1000 VA inrush 8.5 VA sealed for 60 hertz and 100 VA inrush 8.5 VA sealed for 50/60 hertz.


CTA-ID : 11262
Was this helpful?
What can we do to improve the information ?