Technical FAQs

Ask a Question

Is 208 volt replacement control coil available for LC1D1801?

Yes, order LX1D2L6 for 60 hertz. Average coil consumption is 60 VA inrush 7 VA sealed for 50 hertz, 70 VA inrush 7.5 VA sealed for 60 hertz and 70 VA inrush 8 VA sealed for 50/60 hertz.


CTA-ID : 11261
Was this helpful?
What can we do to improve the information ?