Technical FAQs

Ask a Question

What is the maximum length of the rear plunger of an 9066RB1 & RB2?

They are 2.13`` and 3.25`` max., respectively ... both with a .88`` max. travel per digest 170 p. 12-152.


CTA-ID : 11050
Was this helpful?
What can we do to improve the information ?