Technical FAQs

Ask a Question

How can someone get schematics for the ATV66 drive?

Square D does not share board level drawings or schematics.
Here are some reasons.
The drawings may not be up to date.
The drawings often show the nominal ratings for the components but not the tolerance. Our tolerance sometimes exceed the markings on the devices.
Despite the nondisclosure agreements that have been signed some parties have passed on confidential information to competitors.
There should be no need for someone to obtain that level of detail. We provide warranties on our products. Service, repairs and/or replacements are available.

Even with a Non-disclosure agreement these drawings are unlikely to be included.

However, if someone insists then corporate legal office can be contacted. These issues are considered on a case-by-case basis. There is no standard form or procedure.

CTA-ID : 11045
Was this helpful?
What can we do to improve the information ?