Technical FAQs

Ask a Question

Are replacement contacts available for 8965DPR33?

Issue:
What is the part number for replacement contacts for 8965DPR33?

Product Line:
Definite Purpose Starters

Environment:
Products sold and used in the United States

Cause:
Replacement Contacts Needed

Resolution:
Series B: In single pole kits only, order (6) 9998 DRC3 kits.
Series A and Series C devices do not have replacable contacts, as such the 9998DRC3 kit is obsolete.
In single pole kits only, order (6) 9998 DRC3 kits.
 
Was this helpful?
What can we do to improve the information ?