Technical FAQs

Ask a Question

Is it possible to interlock a Mastepact NT and a Masterpact NW by connecting rods?

No. It is NOT possible to carry out an interlocking by connecting rods between a Masterpact NT and a Masterpact NW. This function cannot be carried out with the existing plates. The interlocking by connecting rods is limited to two devices of same family (2 NT, NS or 2 NW). It`s only possible to mix 1 fixed and 1 withdrawable device.


CTA-ID : 10559
Was this helpful?
What can we do to improve the information ?