Technical FAQs

Ask a Question

Can the leads on a SDSA3650 be tapped onto to increase the length of the lead?

No, we do not recommend adding length to the leads. Additional length would change the clamping voltage from published specifications.

CTA-ID : 11010
Was this helpful?
What can we do to improve the information ?