Technical FAQs

Ask a Question

How can a customer test the operation of the motor on a drawout NW breaker if it is removed from the cell?

Use connector # S47849, or borrow one from the cradle to connect to the motor terminals on the breaker. Power can be brought to the motor through this connector for testing.


CTA-ID : 10555
Was this helpful?
What can we do to improve the information ?