Technical FAQs

Ask a Question

We used to have a policy that if a customer wanted to change the rating of a thermal-magnetic CB, we would sell one for the price of a competitive trip unit. Is this still active? Where can I find information on it?

It is called the Exchange Price Guarantee, and is intended to help Square D meet an ``interchangeable trip-unit`` spec for thermal-mag breakers. The details are in the Suplementary Digest.


CTA-ID : 10550
Was this helpful?
What can we do to improve the information ?