Technical FAQs

Ask a Question

What are the dimensions of a SDSA3650 Hardwired Secondary Surge Arrestor?

The module dimensions are 3.00`` High, 3.60`` Wide, 2.64`` Deep. The threaded nipple used for mounting adds an additional .75`` to the depth.

CTA-ID : 11000
Was this helpful?
What can we do to improve the information ?