Technical FAQs

Ask a Question

What are the dimensions of a SDSA1175 Hardwired Secondary Surge Arrestor?

The module dimensions are 2.25`` High, 2.25`` Wide, 1.94`` Deep. The threaded nipple used for mounting adds an additional .75`` to the depth.

CTA-ID : 10999
Was this helpful?
What can we do to improve the information ?