Technical FAQs

Ask a Question

Can the 400 amp main breaker, breaker mounting pan, and deadfront from an NQOD42M400SFB be installed as a main breaker kit on an NQOD54L400 interior?

NO. The main breaker, breaker mouting pan and deadfront portion of an NQOD42M400SFB is designed to be used with an interior that goes into a 6 3/4`` can and the NQOD54L400 is designed to go into a 5 3/4`` can.


CTA-ID : 10313
Was this helpful?
What can we do to improve the information ?