Technical FAQs

Ask a Question

The NA1200AWK enclosure uses the PKOGTA4 ground lug kit. The kit instructions state to mount the PKOGTA4 bracket to a welded bracket in the back of the enclosure. There is not a bracket in the back of the enclosure. What do I do?

On the NA1200AWK, some enclosures may not have the ground bar mounting bracket to accept the PKOGTA4. In those cases, the standard PK32DGTA ground bar will fit in the mounting holes in the back of the enclosure. Just make sure that the mounting screws used do not ``bottom out`` on the wall behind the enclosure before making a secure ground connection.


CTA-ID : 9860
Was this helpful?
What can we do to improve the information ?