Technical FAQs

Ask a Question

Can compression lugs be used on the neutral of an NQOD 225amp panel with sub-feed or thru-feed lugs?

No there isn`t enough clearance at that location of the panel. The standard mechanical sub-feed lug must be provided on the neutral.

CTA-ID : 10088
Was this helpful?
What can we do to improve the information ?