Technical FAQs

Ask a Question

What is the 9007AB43?

This is the 9007AO1 (1 NO contact) with a lever arm pivoting on the left side of the switch, roller on the right end of the lever, so that the device is one-way operation. It has no side mounting plate. the 9007AO23 is essentially the same device, but with a side mounting plate.

CTA-ID : 9950
Was this helpful?
What can we do to improve the information ?