Technical FAQs

Ask a Question

Is replacement control coil available for 8910SYD230V06?

31091-400-57 for 60 hertz or 31074-400-58 for 50 hertz, coil consumption is 1185 VA inrush, 85 VA sealed for 60 hertz applications or 1260 VA inrush, 89 VA sealed for 50 hertz applications.



CTA-ID : 10303
Was this helpful?
What can we do to improve the information ?