Technical FAQs

Ask a Question

Is replacement control coil available for 8910SYD138V06?

31074-400-57 for 60 hertz or 31074-400-58 for 50 hertz, coil consumption is 700 VA inrush, 46 VA sealed for 60 hertz applications or 678 VA inrush, 47 VA sealed for 50 hertz applications.



CTA-ID : 10296
Was this helpful?
What can we do to improve the information ?