Technical FAQs

Ask a Question

What is the part # for a copper neutral for a 30 or 42 ckt NQOD 400 or 600 amp NQOD main lug with thru feed lugs?

Standard aluminum = 80110-413-50

Copper base w/ aluminum branch terminations = 80110-413-51

Copper base w/ copper branch terminations = 80110-793-50

Available branch terminations are:

Aluminum main lugs: (4) #1/0 - 750MCM or (8) #1/0 - 300MCM
Copper main lugs: (4) #2 - 600MCM

Branch:

(4) #4 - 300MCM
(1) #14 - 2/0
(29) #4 - 14

Revised 4/27/04



CTA-ID : 10084
Was this helpful?
What can we do to improve the information ?