Technical FAQs

Ask a Question

Are IEC breakers, like the C1251 80% or 100% rated?

The 80% rating applies only to UL listed breakers. There is no restriction to applying IEC rated breakers at 100% of their amp rating.


CTA-ID : 10077
Was this helpful?
What can we do to improve the information ?