Technical FAQs

Ask a Question

What is a QOUR120 and what is the replacement?

The QOUR120 was a Series 1 QOU with factory only reversed lugs. The replacement is the Series 3 QOUR120 which has factory reversed lugs. However, these lugs can be field reversible for forward or reverse connection. Therefore, you could also order a QOU120 and field reverse the lugs.


CTA-ID : 9843
Was this helpful?
What can we do to improve the information ?