Technical FAQs

Ask a Question

I can use the SN1000MA neutral kit with the NEMA 1 rated ME1000S enclosure.

The footnote on page 6-48 (DIGEST 172) is correct.
After checking the wiring diagram (40268-726-02),
the only Neutral listed for use in this ME1000S
circuit breaker enclosure is SN1000MA.
This wiring diagram does not list alternate neutral SNC800LX,
Ground Bar Kit for this enclosure is PKGTA-4.

CTA-ID : 9836
Was this helpful?
What can we do to improve the information ?