Technical FAQs

Ask a Question

Can I use the GFM250 add-on ground-fault module with a two pole KAL/KHL/KCL/KIL breaker?

Yes. The system must be a grounded system.


CTA-ID : 9829
Was this helpful?
What can we do to improve the information ?