Technical FAQs

Ask a Question

What is the part number for the neutral assembly used on 225A NQOD panels w/ 42 or 54 ckts?

Standard Aluminum = 80110-201-78

Copper base w/ aluminum branch terminations = 80110-201-80

Copper base w/ copper branch terminations = 80110-201-79

Available terminations are:

Al main lug: (1) #6 - 300MCM
Cu main lug: (1) #6 - 250MCM

Branch:

(45) #4 - 14



Revised 4/27/04




CTA-ID : 10068
Was this helpful?
What can we do to improve the information ?