Technical FAQs

Ask a Question

What are the repair parts for the DTU463AWK, series F5? (may be shown as F05)

The repair parts for the DTU463AWK, series F5 (F05) are as follows. No other parts are available. (NOTE: Descriptions below of ``left side`` and ``right side`` mean your left or right as you face the switch.)
-Left Side Line Base - 40566-713-50 (one each upper and lower. Order arc suppressor, load lugs, and wire assembly separately. NOTE: thermoplastic cam between right and left line base may also be required.).
-Right Side Line Base - 40566-826-50 (one each upper and lower. Order arc suppressor, load lugs, and wire assembly separately. NOTE: thermoplastic cam between right and left line base may also be required.).
-Thermoplastic Cam between Left and Right Line Bases - 40567-028-01.
-Line Base mounting screws - 40205-151-01 (requires 3 per line base).
-Arc Suppressor Assembly - 40566-355-50 (requires 1 per line base).
-Arc Suppressor mounting screw - 40205-145-01 (requires 1 per arc suppressor).
-Wire Assembly Line Base Left Side 40566-218-50 and Right Side 40566-883-50 (requires 1 per phase. Includes cable factory connected mechanical lug at one end and at other end a crimped connector. Use mounting screws of line and load lugs.)
-Lug assembly - CL10F (includes 6 lugs)
-Line, Load Lug mounting screw - 40205-142-02
-Ground Lug - 40251-018-51 (per lug).
-Ground Lug mounting screw - 40205-135-03
-Switch Mechanism - 40566-469-50 (each for upper and lower).
-Linkage Assembly - 40566-827-50 (links together upper and lower switch mechanisms). Also replace linkage assembly rubber gaskets.
-Linkage Assembly Rubber Gaskets - 40503-228-01 (3 total required)
-Linkage Assembly mounting screws - 22999-405-62 (requires 7).
-Handle - 40566-887-50 (In addition, handle gasket required. Lockplate gasket may also need replacing)
-Handle gasket - 40566-086-01
-Lockplate - 40566-733-01 (In addition, lockplate gasket required.)
-Lockplate gasket - 40566-086-01 (requires 1)
-Lockplate mounting screws - 22999-405-62 (requires 2).



CTA-ID : 9935
Was this helpful?
What can we do to improve the information ?