Technical FAQs

Ask a Question

Did the old NA1200AWK circuit breaker enclosure provide a means to lock the circuit breaker ON or OFF?

Issue:
Product design features

Product Line:
Circuit Breaker Enclosures

Resolution:
The NA1200AWK is an old obsolete circuit breaker enclosure that is NO longer available.

The NA1200AWK circuit breaker enclosure was not an externally operable device. The enclosure door must be opened to operate the enclosed NAL, NHL or NXL breaker. The enclosure is equipped with a vault handle on the enclosure door, which is lockable. This vault handle locks the enclosure door closed only and does not perform any locking function of the Circuit Breaker. However, a handle padlock attachment, HPANE, was included with the NA1200AWK enclosure for field installation on the Circuit Breaker, if required, for padlocking the circuit breaker ON or OFF.


CTA-ID : 9824
Was this helpful?
What can we do to improve the information ?