Technical FAQs

Ask a Question

Is there an isolated alarm circuit available for the LR3D OLR?

The IEC LRD, LR2D, LR3D overload relays are provided with a normally open contact as standard. This contact can be used for an alarm circuit if so desired.

CTA-ID : 9820
Was this helpful?
What can we do to improve the information ?