Technical FAQs

Ask a Question

If I select a cylinder lock in Product Selectors, will this give me the capability of interlocking two breakers in a dual source scheme so that only one breaker can be on at a time?

A cylinder lock is a lock that is built into the breaker itself and is not to be used in situations where there are 2 separate power sources coming into a panel. Key interlocks are used in these situations. Choosing a key interlock is not product selectable and it must be entered in Special Pricing Notepad using pricing from the PB-1 pricing brochure. Keep in mind that it does require 3`` of space adjacent to the breaker for the mounting bracket.


CTA-ID : 9813
Was this helpful?
What can we do to improve the information ?