Technical FAQs

Ask a Question

Is replacement control coil available for 8910DPA122V02?

31074-400-38 for 60 hertz or 31074-400-39 for 50 hertz, coil consumption is 700 VA inrush, 46 VA sealed for 60 hertz applications or 678 VA inrush, 47 VA sealed for 50 hertz applications.


CTA-ID : 10276
Was this helpful?
What can we do to improve the information ?