Technical FAQs

Ask a Question

How many inches of unit mounting space is taken up by a branch mounted TVSS unit installed on an I-Line interior?

13.5`` of unit mounting space is required for a branch mounted TVSS unit in I-Line construction. The unit is not available on HCN type interiors.


Revised 3/10/04




CTA-ID : 10053
Was this helpful?
What can we do to improve the information ?