Technical FAQs

Ask a Question

What do the letters NL on the end of an NQOD panelboard interior part number (ex. NQOD442L225NL) signify ?

The letters NL signify that the interior is rated for Non-Linear Loads (200% rated neutral).

Revised 3/9/04

CTA-ID : 9805
Was this helpful?
What can we do to improve the information ?