Technical FAQs

Ask a Question

What are the repair parts for a PAK10C, Series E02, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Cover - 4054000501
Cover Mounting Screw - 2142717161 (2 req`d)
Interior Trim - 4054026401
Interior Trim Mounting Screw - 4020513001K (1 req`d)
Interior Assembly - 4054026050 (Includes the Base Assy, Circuit Breaker and Receptacle listed below. Also includes the neutral assembly, not listed separately.)
Base Assembly - 4054025950
Circuit Breaker - QO120GFI
Receptacle - 4054001450
Neutral Bonding Screw - 4028318561
Ground Bar - 4023017383
Ground Bar Mounting Screw - 4020547201 (1 req`d)
Closing Cap - BCAP
Closing Cap Mounting Screw - 2142720241
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 9803
Was this helpful?
What can we do to improve the information ?