Technical FAQs

Ask a Question

What are the repair parts for the DTU462, series F5? (may be shown as F05)

Issue:
Repair parts

Product Line:
Double Throw Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:

The repair parts for the DTU462, series F5 (F05) are as follows. No other parts are available. (NOTE: Descriptions below of ``left side`` and ``right side`` mean your left or right as you face the switch.)
-Left Side Line Base - 40566-255-50 (one each upper and lower. Order arc suppressor, load lugs, and wire assembly separately. NOTE: thermoplastic cam between right and left line base may also be required.).
-Right Side Line Base - 40566-250-50 (one each upper and lower. Order arc suppressor, load lugs, and wire assembly separately. NOTE: thermoplastic cam between right and left line base may also be required.).
-Thermoplastic Cam between Left and Right Line Bases - 40567-028-01.
-Line Base mounting screws - 40205-151-01 (requires 3 per line base).
-Arc Suppressor Assembly - 40566-355-50 (requires 1 per line base).
-Arc Suppressor mounting screw - 40205-145-01 (requires 1 per arc suppressor).
-Wire Assembly Line Base Left Side 40567-326-50 and Right Side 40566-097-50 (requires 1 per phase. Includes cable factory connected mechanical lug at one end and at other end a crimped connector. Use mounting screws of line and load lugs.)
-Line and Load Lug Assembly - 40251-016-52 (per lug - line, load)
-Line, Load Lug mounting screw - 40205-142-02
-Ground Lug - 40251-016-52 (per lug).
-Ground Lug mounting screw - 40205-135-03
-Switch Mechanism - 40566-469-50 (each for upper and lower).
-Linkage Assembly - 40566-827-50 (links together upper and lower switch mechanisms)
-Linkage Assembly mounting screws - 22999-405-62 (requires 7).
-Handle - 40566-887-50
-Lockplate - 40566-733-01
-Lockplate mounting screws - 22999-405-62 (requires 2).



CTA-ID : 9930
Was this helpful?
What can we do to improve the information ?