Technical FAQs

Ask a Question

Is a service maual showing how to disassemble and reassemble an SE breaker available?

The SE circuit breaker is a UL listed MCCB, and as such cannot be disassembled, reassembled, and placed back into service. The molded case is sealed and if it is ever opened up, the circuit breaker loses all of its certifications, warranties, and is considered to be unsafe.

CTA-ID : 9802
Was this helpful?
What can we do to improve the information ?