Technical FAQs

Ask a Question

What is the failure mode of UVR for the Compact NS breakers? Will it open the breaker if the coil burns out?<br />

Yes, it is ``fail safe``. The coil must be energized for the breaker to close.


CTA-ID : 9799
Was this helpful?
What can we do to improve the information ?