Technical FAQs

Ask a Question

What are the repair parts for the HU362A, series F5? (may be shown as F05)

Issue:
Repair Parts

Product Line:
Heavy Duty Safety Switch

Cause:
Maintenance

Resolution:
The replacement parts for the HU362A, series F5 (F05) are as follows. No other parts are available.

Interior Kit - HSIU3606CF (includes line base Assembly, mechanism, arc suppressor, all mtg. hardware and instructions).
Arc Suppressor Kit - HAS0610F (includes arc suppressor, mtg. hardware and instructions).
Lug Kit - CL0306F (includes 6-lugs and mtg. hardware)
Handle/Mechanism Kit - HM0610F (includes handle, mechanism, lockplate, gasket, all mtg. hardware and instructions).


CTA-ID : 10033
Was this helpful?
What can we do to improve the information ?