Technical FAQs

Ask a Question

What are the repair parts for the H462AWK, series F5? (may be shown as F05)

Issue:
Repair Parts

Product Line:
Heavy Duty Safety Switch

Cause:
Maintenance

Resolution:
The replacement parts for the H462AWK, series F5 (F05) are as follows. No other parts are available.

Interior Kit - HSIF4606CF (includes line and load base Assemblies, mechanism, arc suppressor, all mtg. hardware and instructions).
Load Base Kit - HLB2606CF - TWO kits required (includes load base, mtg. hardware and instructions)
Arc Suppressor Kit - HAS0610F - TWO kits required (includes arc suppressor, mtg. hardware and instructions).
Lug Kit - CL0306F - TWO kits required (includes 6-lugs and mtg. hardware)
Handle/Mechanism Kit - HM0610F (includes handle, mechanism, lockplate, gasket, all mtg. hardware and instructions).


CTA-ID : 10032
Was this helpful?
What can we do to improve the information ?