Technical FAQs

Ask a Question

What are the repair parts for a PAK72CGFI, Series E03, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Cover - 4054025101
Cover Mounting Screws - 2142717161 (2 req`d)
Interior Trim - 4054029601
Interior Trim Mounting Screw - 4020513001K (2 req`d)
Interior Assembly - (2) 4054009150 and 4054029150 (Includes the Base Assy, Circuit Breaker(s) and Receptacle(s) listed below. Also includes the neutral assembly, not listed separately)
Interior Assembly Mounting Screw - 2142217101 (2 req`d)
Neutral Assembly Mounting Screw - 2159417121
Base Assembly - 4054006850
Circuit Breaker - (2) QO120GFI and QO220GFI
Receptacle - (2) 4054001450 (125 volt/20 amp) and 4054004351 (125/250 volt/20 amp)
Receptacle Mounting Screw - 2190312160 (2 req`d for each 125 volt/20 amp receptacle, 2 req`d for the 125/250 volt/20 amp receptacle)
Receptacle Mounting Spring Clip - 2330100001 (2 req`d for each 125 volt/20 amp receptacle only - not required for the 125/250 volt/20 amp receptacle)
Ground Bar - 4023089855
Ground Bar Mounting Screw - 2159414200
Neutral Bonding Strap Assembly - 4028359250
Closing Cap - BCAP
Closing Cap Mounting Screw - 2142720241
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 9791
Was this helpful?
What can we do to improve the information ?