Technical FAQs

Ask a Question

What are the repair parts for the HU661AWK, series F5? (may be shown as F05)

The replacement parts for the HU661AWK, series F5 (F05) are as follows. No other parts are available.

Complete Interior kit - HSIU6603606CF (Includes line base assembly, arc suppressor, mechanism, all mounting hardware and instructions)
Arc Suppressor kit - HAS0610F- TWO required (includes arc suppressor, mtg. hardware & instructions)
Lug kit - CL0306F- TWO required (includes 6 lugs, mtg. hardware & instructions)
Handle/Mechanism kit - HM0610F (includes handle, mechanism, gaskets, lockplate, mtg. hardware & instructions)

CTA-ID : 10023
Was this helpful?
What can we do to improve the information ?