Technical FAQs

Ask a Question

Why do we offer two different Nema Type 1 box depths for our QMB panels?

If a 4-piece trim is called for the depth is standard 11 1/2``. If a trim with door is called for the box depth must increase to 18`` so the door won`t interfere with the handles on the switches.

CTA-ID : 9774
Was this helpful?
What can we do to improve the information ?