Technical FAQs

Ask a Question

Is the GA12TPM test panel optional for the GROUND-CENSOR Type GA gound fault system?

Yes. It is optional and not required.


CTA-ID : 9748
Was this helpful?
What can we do to improve the information ?