Technical FAQs

Ask a Question

What are the repair parts for the H361A, series F5? (may be shown as F05)

The replacement parts for the H361A, series F5 (F05) are as follows. No other parts are available.

Line Base Assembly - 40566-429-50 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 40560-027-50 (requires one per switch)
Arc Suppressor Assembly - 40566-694-51 (requires one per switch)
Lug Assembly - CL0306F (includes 6 lugs)
Switch Mechanism - 40566-107-50
Handle Assembly - 4056684150K
Handle Gasket - 40566-031-01
Lockplate - 40566-376-01
Line & Load base mounting screw - 40205-160-01 (3 for line & 2 for load)
Arc Suppressor mounting screw - 40205-145-01 (1 required)
Lockplate mounting screw - 22999-405-62 (2 required)


CTA-ID : 10004
Was this helpful?
What can we do to improve the information ?