Technical FAQs

Ask a Question

Can you use the Ethernet Communication Module (ECM)-2000 or ECM-200RM to communicate to Micrologic trip units?

No, the ECM does not provide a broad enough address range to communicate to each portion of the trip units. The ECM address range is 1 through 32.

CTA-ID : 9743
Was this helpful?
What can we do to improve the information ?